Write-only |
About VISAPassthrough |
Description |
Closes the specified remote VISA session. VISA sessions should always be closed when you are finished communicating with the remote device. Use this command to close (end) each VISA session that was opened successfully using the Open method. If you have more than one open session, and need to close them all at the same time, it may be faster and easier to use the Reset method. |
VB Syntax |
Vpassthru.Close visaID |
Variable |
(Type) - Description |
|
Vpassthru |
(object) - A VISAPassthrough object |
visaID |
(long) VISA session number (see Open method). |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Vpassthru.Close 2 |
C++ Syntax |
HRESULT Close(long session_num) |
Interface |
IVISAPassthrough |