Write-only |
About Cal Sets |
Description |
Computes error terms for the caltype specified by a preceding OpenCal Set call. The Cal Set must first be opened using OpenCalSet. If this call has not been made, the following error is issued: E_NA_Cal Set_ACCESS_DENIED The standards data required for the CalType must be available in the Cal Set or this error will be returned: E_NA_STANDARD_NOT_FOUND. Note: Error term computation requires data for the actual calibration kit standards from the current kit definition. ComputeErrorTerms assumes that the standards were acquired using only one standard per class. |
VB Syntax |
CalSet.ComputeErrorTerms |
Variable |
(Type) - Description |
|
CalSet |
(object) - A Cal Set object |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
CalSet.ComputeErrorTerms |
C++ Syntax |
HRESULT ComputeErrorTerms( ) |
Interface |
ICalSet |