Write-Read
 

ConfigEnhancedNB Method - Superseded


Description

Note: This command is replaced by ConfigEnhancedNB2 Method

This subroutine determines, then returns, the proper configuration for pulsed measurements on the PNA-X ONLY using the spectral nulling technique.  The configuration returned needs to be sent to the VNA and any other related external equipment.

The routine will take a desired Pulse Repetition Frequency (PRF) and measurement IFBW and return a possibly modified PRF and IFBW for proper pulsed operation on the VNA.

 VB Syntax

Pulsed.ConfigEnhancedNB (PRF, BW, PhysicalIF, NCO, Stage1TapArray, Stage2TapArray, Stage3TapArray, FixedPRF)

Variable

(Type) - Description

Pulsed

(interface)  An interface to the agilentpnapulsed.dll application interface.

PRF

(Double)  The Pulse Repetition Frequency.

[out]  The pulse repetition frequency that has been optimized for use with the VNA.  NOTE: This value may be different from the value requested.

[in]  The desired pulse repetition frequency.

BW

(Long)  The VNA IF Bandwidth.

[out]  The VNA IF bandwidth that has been optimized for use with the VNA.  NOTE: This value may be different from the value requested. Zero (0) is returned if no solution is found for the specified PRF and BW.

[in]  The desired VNA IF bandwidth.

PhysicalIF

(Double)  Returns physical intermediate frequency.

NCO

(Double)  Returns numeric controlled oscillator frequency.

Stage1TapArray

(Long array) Returns the stage 1 filter coefficients

Stage2TapArray

(Long array) Returns the stage 2 filter coefficients

Stage3TapArray

(Long array) Returns the stage 3 filter coefficients

FixedPRF

(Boolean)  

1 (True)  Signals the .DLL routine to NOT adjust the PRF value; rather adjust ONLY the IF Bandwidth. This is the default setting.

0 (False)  Adjust both the PRF and IF Bandwidth values as necessary.

Return Type

Not Applicable

Default

Not Applicable

C++ Syntax

HRESULT ConfigEnhancedNB(double *pPRF, long *pBW, double *pIF, double *pNCO, double *pStg1, double *pStg2, double *pStg3)

Interface

AgilentPNAPulsed.Application