Write-only |
About Cal Sets |
Description |
Creates a new Cal Set. The new cal set is initialized with the stimulus settings from the channel whose number is passed as the argument to this method. Stimulus settings include frequency, bandwidth, number of points, and so forth. Use this method when you want to manually upload data to the Cal Set using the returned ICal Set interface handle.. The channel number does not restrict the usage of this Cal Set on any other channel. It simply provides a link to the originating channel so that the stimulus values can be stored in the Cal Set. Note: Be sure to SAVE the CalSet you are creating. Use ICalSet::Save. |
VB Syntax |
calMgr.CreateCalSet (chan) |
Variable |
(Type) - Description |
|
calMgr |
(object) - A CalManager object |
|
chan |
(long) - channel number of the new Cal Set. |
Return Type |
ICal Set Interface |
Default |
Not Applicable |
Example |
calMgr.CreateCalSet 1 |
C++ Syntax |
HRESULT CreateCalSet( long ChannelNumber, ICal Set** pCal Set); |
Interface |
ICalManager |