Write-only |
About Differential IQ |
Description |
Create a new parameter for Differential IQ channel. Use CreateCustomMeasurementEx Method to create a new trace with the new parameter. Use Change Parameter Method to change the parameter of one of the existing traces to the new parameter. |
VB Syntax |
DIQ.DefineParameter (name, expression) |
Variable |
(Type) - Description |
|
DIQ |
|
|
name |
(String) Parameter name. Note: Do not use underscores in the parameter name. For example, b2_f1 cannot be used as a parameter name. However, b2f1 is a valid parameter name. |
|
expression |
(String) Parameter expression using receiver names and mathematical expressions. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Diq.DefineParameter "myNewParam","(a1_F1+b1_F2)/c1" app.ActiveMeasurement.ChangeParameter "myNewParam",1 |
C++ Syntax |
HRESULT DefineParameter(BSTR name,BSTR expression); |
Interface |
IDIQ |