Write-only |
About Differential IQ |
Description |
Deletes the specified frequency range. On the Measurement Setup dialog this is the Remove setting. |
VB Syntax |
DIQ.DeleteRange (n) |
Variable |
(Type) - Description |
|
DIQ |
|
|
n |
(Long) Frequency range number to delete. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
diq.DeleteRange 2 'removes frequency range 2 |
C++ Syntax |
HRESULT DeleteRange(long range); |
Interface |
IDIQ |