Write-only |
About Cal Window |
Description |
Set the 'show' state of the window to be displayed during a calibration. When this command is sent, the specified window is 'flagged' to be shown during calibration. The flag is cleared when the window is closed. A Preset or Instrument State Recall also closes the window. If the same window number is reopened, this command must be sent again to show the window during a calibration. The flag is NOT saved with an instrument state. Send this command for each additional window to show during a calibration. |
VB Syntax |
calMgr.DisplayNAWindowDuringCalAcquisition (winNum, State) |
Variable |
(Type) - Description |
|
calMgr |
(object) - A CalManager object |
|
winNum |
(long) - Window number to show during a calibration. The calibration window will also be shown with this window. The window must already be created. Use NaWindows.count or app.WindowNumber to read existing window numbers. |
|
state |
(Boolean) Window state. Choose from: True - Show the specified window during calibration. False - Do NOT show the specified window during calibration. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Example |
calMgr.DisplayNAWindowDuringCalAcquisition 2,True |
C++ Syntax |
HRESULT DisplayNAWindowDuringCalAcquisition( long WinNum, VARIANT_BOOL bVal); |
Interface |
ICalManager5 |