Write-only |
About Macros |
Description |
Executes a Macro (shortcut) stored in the analyzer. Use app.getShortcut to list existing macros. Use app.putShortcut to associate the macro number with the file. |
VB Syntax |
app.ExecuteShortcut index |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
index |
(long integer) - Number of the macro stored in the analyzer. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.ExecuteShortcut 1 |
C++ Syntax |
HRESULT ExecuteShortcut(long index) |
Interface |
IApplication |