Read-only |
About Gain Compression |
Description |
For a specified data point, returns the imaginary part of the specified Gain Compression data. If correction is on, corrected data are returned. Otherwise, raw data are returned. Can be used with Smart and 2D sweeps.
|
VB Syntax |
data = gca.GetDataIm stim, dPoint, param |
Variable |
(Type) - Description |
|
data |
Variant array in which to store returned measurement data. |
|
gca |
A GainCompression (object) |
|
stim |
(NAGCAIndexSelect)
|
|
dPoint |
Data point (Frequency or Power) for which data is returned. |
|
param |
Parameter of data to return. Not case-sensitive. Choose from:
|
Return Type |
Variant Array |
Default |
Not Applicable |
Examples |
For the fifth frequency data point, returns 'Power Output' imaginary (phase) data from all power stimulus values. If there are 30 power sweep points, 30 values are returned. data = gca.GetDataIm naFrequencySelect, 5, "pout" For the 30th stimulus power data point, returns 'Power Output' imaginary (phase) data from all frequency stimulus values. If there are 201 frequency sweep points, 201 values are returned. data = gca.GetDataIm naPowerSelect, 30, "pout" Note: For 2D sweeps, the number of data points returned / freq may vary. Learn more. |
C++ Syntax |
HRESULT GetDataIm(tagNAGCAIndexSelect index_select, int index,BSTR data_name, VARIANT* pData); |
Interface |
IGainCompression |