Read-only |
About Gain Compression |
Description |
Reads the REAL part of the data acquired from any GCA sweep. Previously 2D sweep only. Note: For 2D sweeps, the number of data points returned / freq may vary. Learn more. |
VB Syntax |
data = gca.GetDataRe stim, dPoint, param |
Variable |
(Type) - Description |
|
data |
Variant array in which to store returned measurement data. |
|
gca |
A GainCompression (object) |
|
stim |
(NAGCAIndexSelect)
|
|
dPoint |
Data point (Frequency or Power) for which data is returned. |
|
param |
Parameter of data to return. Not case-sensitive. Choose from:
|
Return Type |
Variant Array |
Default |
Not Applicable |
Examples |
For the fifth frequency data point, returns 'Power Output' REAL data from all power stimulus values. If there are 30 power sweep points, 30 values are returned. data = gca.GetDataRe naFrequencySelect, 5, "pout"
For the 30th stimulus power data point, returns 'Power Output' REAL data from all frequency stimulus values. If there are 201 frequency sweep points, 201 values are returned. data = gca.GetDataRe naPowerSelect, 30, "pout" Note: For 2D sweeps, the number of data points returned / freq may vary. Learn more. |
C++ Syntax |
HRESULT GetDataRe(tagNAGCAIndexSelect index_select, int index,BSTR data_name, VARIANT* pData); |
Interface |
IGainCompression |