Description
|
Returns an NA_IPConfiguration data structure which contains information about the current status of the VNA’s computer networking configuration. This is the same set of information that is returned in a single string by the LANConfiguration property.
|
VB Syntax
|
value = app.GetIPConfigurationStruct
|
Variable
|
(Type) - Description
|
|
value
|
(NA_IPConfiguration) Variable to receive the VNA IP (LAN) configuration information.
|
|
app
|
An Application (object)
|
Return Type
|
NA_IPConfiguration
|
Default
|
Not Applicable
|
Examples
|
Dim networkConfigInfo As NA_IPConfiguration
networkConfigInfo = app.GetIPConfigurationStruct()
MsgBox “Host name = ” & networkConfigInfo.HostName
MsgBox “Domain name = ” & networkConfigInfo.DomainName
MsgBox “IP address = ” & networkConfigInfo.IPAddress
If Not networkConfigInfo.DHCPEnabled Then
MsgBox “IP address is static”
Else
MsgBox “IP address is dynamic”
End If
MsgBox “Subnet mask = ” & networkConfigInfo.SubNet
MsgBox “Gateway = ” & networkConfigInfo.DefaultGateway
MsgBox “Primary DNS server = ” & networkConfigInfo.DNSServer1
MsgBox “Secondary DNS server = ” & networkConfigInfo.DNSServer2
MsgBox “First suffix in DNS suffix search order = ” & networkConfigInfo.DNSSuffix1
MsgBox “Second suffix in DNS suffix search order = ” & networkConfigInfo.DNSSuffix2
MsgBox “Primary WINS server = ” & networkConfigInfo.PrimaryWINSServer
MsgBox “Secondary WINS server = ” & networkConfigInfo.SecondaryWINSServer
MsgBox “Network adapter device ID = ” & networkConfigInfo.DeviceID
MsgBox “Description of network adapter = ” & networkConfigInfo.Description
MsgBox “MAC address = ” & networkConfigInfo.MacAddress
|
C++ Syntax
|
HRESULT GetIPConfigurationStruct (tagNA_IPConfiguration * pIPConfig);
|
Interface
|
IApplication14
|