Write-only |
About Modifying Cal Kits |
Description |
Returns a handle to a calibration standard for modifying its definitions. To select a standard for performing a calibration (use Calibrator.AquireCalStandard). |
VB Syntax |
calkit.GetCalStandard(index) |
Variable |
(Type) - Description |
|
calkit |
A calKit (object) |
|
index |
(long) - Number of calibration standard. Choose 1 to 30; (there are 30 cal standards in every kit). |
Return Type |
calStandard |
Default |
Not Applicable |
Examples |
Dim short As CalStandard |
C++ Syntax |
HRESULT GetCalStandard(long standardNumber, ICalStandard **pCalStd) |
Interface |
ICalKit |