Read-only |
Data Access Map |
Description |
Retrieves variant data from the specified location in your choice of formats. The VNA returns complex trace data which is ratioed if required by the measurement parameter, such as S11 or A/B. Otherwise it is raw receiver data, such as A or B. Equation Editor Notes:
|
VB Syntax |
data = meas.getDataByString location, format |
Variable |
(Type) - Description |
|
data |
(variant) - Array to store the data. |
|
meas |
(object) - A Measurement object |
|
location |
(string) – Name of the buffer to be read. Choose from: "naRawData" "naCorrectedData" "naMeasResult" "naRawMemory" "naMemoryResult" "naDivisor" - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. See Data Access Map |
|
format |
(enum NADataFormat) - Format in which you would like the data. It does not have to be the displayed format. Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade * Specify Smith or Polar formats to obtain complex data pairs, which require a two-dimensional array varData (numpts, 2) to accommodate both real and imaginary data. All scalar formats return a single dimension varData(numpts). |
Return Type |
Variant array |
Default |
Not Applicable |
Examples |
meas.getDataByString “naMeasResult”, naDataFormat_Phase |
C++ Syntax |
HRESULT getDataByString( BSTR location, tagDataFormat dataFormat, VARIANT * pData ); |
Interface |
IMeasurement |