Read-only |
Data Access Map |
Description |
Retrieves variant data from the specified location in your choice of formats. To get smoothed data from any of the specified locations, the format must be the same as the displayed format. The VNA returns complex trace data which is ratioed if required by the measurement parameter, such as S11 or A/B. Otherwise it is raw receiver data, such as A or B. This method returns a variant which is less efficient than methods available on the IArrayTransfer interface. If you plan to Put this data back into analyzer, putDataComplex (variant data) method requires complex, two-dimensional data. Therefore, request the data in Polar format. Equation Editor Notes:
|
VB Syntax |
data = meas.GetData location, format |
Variable |
(Type) - Description |
|
data |
Variant array to store the data. |
|
meas |
A Measurement (object) |
|
location |
(enum NADataStore) - Where the data you want is residing. See Data Access Map. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult 3 - naRawMemory 4 - naMemoryResult 5 - naDivisor When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. |
|
format |
(enum NADataFormat) - Format in which you would like the data. It does not have to be the displayed format. Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar* 4 - naDataFormat_Smith* 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade * Specfiy Smith or Polar formats to obtain complex data pairs, which require a two-dimensional array varData (numpts, 2) to accommodate both real and imaginary data. All scalar formats return a single dimension varData(numpts). naDataFormat_Phase and naDataFormat_PhaseUnwrapped returns degrees. However, putDataScalar method accepts data in radians (not degrees) and displays in degrees. |
Return Type |
Variant array - automatically dimensioned to the size of the data |
Default |
Not Applicable |
Examples |
Dim varData As Variant |
C++ Syntax |
HRESULT getData(tagNADataStore DataStore, tagDataFormat DataFormat, VARIANT *pData) |
Interface |
IMeasurement |