Read-only |
Description |
Note: This command replaces Get SnPData. This command is more explicit regarding the data to be returned, and works for VNAs with multiport test sets. Reads SnP data for the measurement by specifying the VNA port numbers. Learn more about SnP that is returned from the VNA. |
VB Syntax |
data = meas.GetSnPDataWithSpecifiedPorts ports |
Variable |
(Type) - Description |
|
data |
(Variant) array to store the data. |
|
meas |
A Measurement (object) |
|
ports |
(Variant Array) One-dimensional array containing the list of port numbers for which data is required. |
Return Type |
Variant - 3 dimensional array.
For example: Data(0,5,1) returns the imaginary part of the fifth data point of S11 (if the s2p request includes port #1) |
Default |
Not Applicable |
Example |
'This VBScript example can be pasted into a notepad file and run on the VNA as a macro. Learn how. Dim pna Dim meas Dim param Dim point Dim snp Dim ports 'List the port numbers for required data ports = Array(3,4) Set pna = CreateObject("AgilentPnA835x.application") Set meas = pna.ActiveMeasurement 'limit amount of data to display set chan=pna.ActiveChannel chan.NumberOfPoints=2 snp = meas.GetSnPDataWithSpecifiedPorts (ports) ' returns a 3 dimensional array ' snp(param,point,data pair) '------------------------------------- ' show me the data For param = LBound(snp, 1) To UBound(snp, 1) MsgBox ("Parameter: " & (param + 1)) For point = LBound(snp, 2) To UBound(snp, 2) MsgBox "Point:" & (point + 1) & " " & snp(param, point, 0) & "," & snp(param, point, 1) Next Next |
C++ Syntax |
HRESULT GetSnpDataWithSpecifiedPorts(VARIANT portsToMeasure,VARIANT* response); |
Interface |
IMeasurement7 |