Write-only |
About LXI |
Description |
Performs an initialization (reset) of the VNA’s LAN configuration, as dictated by Section 8.14 of the LAN eXtensions for Instrumentation (LXI) standard (Version 1.1). This performs the same operation as pressing the LAN Reset button on the VNA LAN Status dialog. |
VB Syntax |
app.LANConfigurationInitialize |
Variable |
(Type) - Description |
|
app |
An Application (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.LANConfigurationInitialize |
C++ Syntax |
HRESULT LANConfigurationInitialize (); |
Interface |
IApplication13 |