Read-Write |
About the Cal Wizard |
Description |
Launches the S-parameter Cal Wizard on the VNA and does not return until the Cal Wizard is dismissed. To launch the Cal Wizard for a VNA Application, use the LaunchDialog Method. Note: The Cal Wizard operates on the active measurement. Therefore, activate the measurement to be calibrated before launching the Cal Wizard. |
VB Syntax |
success = app.LaunchCalWizard (newCS) |
Variable |
(Type) - Description |
|
success |
(boolean) - variable to store the returned value True - The Cal was completed False - The Cal was canceled without completing the calibration. |
|
app |
An Application (object) |
|
newCS |
(boolean) True - Cal will be performed on a new Cal Set. False - Cal will be performed using the existing Cal Set assigned to the channel. If no Cal Set is found, a new Cal Set will be created. |
Return Type |
Boolean |
Default |
Not Applicable |
Example |
dim bSuccess as boolean |
C++ Syntax |
HRESULT LaunchCalWizard(VARIANT_BOOL bCalsuccess) |
Interface |
IApplication |