Write-only |
About 4-Port Fixturing |
Description |
Set the port mapping for a 4-port SNP file to be embedded. To read port mapping, use NetworkPortMapA, NetworkPortMapB, NetworkPortMapC, NetworkPortMapD. |
VB Syntax |
fixture.NetworkPortMap network, inA, inB, outA, outB |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
network |
Network position. Choose from 1 or 2. |
|
inA, inB, outA, outB |
Port Mapping. Use four port numbers in any order. |
Return Type |
Not Applicable. |
Default |
1,2,3,4 |
Examples |
fixture.NetworkPortMap 1,1,3,2,4 |
C++ Syntax |
HRESULT NetworkPortMap(short Net, *Long inA, *Long inB,* Long outA,* Long outB,) |
Interface |
IFixturing6 |