Write-only |
About Dynamic Range |
Description |
A function that returns the previous IF Bandwidth value. Use to retrieve the list of available IFBandwidth settings. |
VB Syntax |
chan.Previous_IFBandwidth bw |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
bw |
(double) - The argument that you use to send an IFBandwidth. The function uses this argument to return the previous IFbandwidth. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Public pnbw As Double 'declare variable outside of procedure PreBW = chan.IFBandwidth 'put the current IFBW in PreBW |
C++ Syntax |
HRESULT Previous_IFBandwidth (double *pVal) |
Interface |
IChannel |