Write-only |
About Cal Sets |
Description |
Puts error term data into the Cal Set. Learn more about Reading and Writing Cal Data |
VB Syntax |
ICalData3.PutErrorTermComplexByString errorName, lnumPoints, real(0), imag(0) |
Variable |
(Type) - Description |
|
ICalData3 |
An ICalData3 pointer to a Cal Set object. |
|
errorName |
(String) The string name used to identify a particular error term in the Cal Set. An example string for port 3 directivity in a full 2 port cal might be "Directivity(3,3)". To determine the string names of error terms, see GetErrorTermList2. |
|
lnumPoints |
(Long) The number of data points in the real and imaginary arrays. |
|
real |
(Single) The real component of the complex data. |
|
imag |
(Single) The imaginary component of the complex data. Note: The size of the real and imaginary arrays should be the same. |
Return Value |
Not Applicable |
Default |
Not Applicable |
Examples |
|
C++ Syntax |
HRESULT PutErrorTermComplexByString( BSTR bufferName, long lnumPoints, float* real, float* imag); |
Interface |
ICalData3 |