Write-only |
Data Access Map |
Description |
Puts complex data into the specified location. This method forces the channel into Hold mode to prevent the input data from being overwritten. The data is processed and displayed. Data put in the naRawData store will be re-processed whenever a change is made to the measurement attributes such as format or correction. Data put in the naMeasResult store will be overwritten by any measurement attribute changes (such as moving a marker). Note: This method uses NAComplex which is a user-defined data type. If you cannot or prefer not to use this data type, use the putComplex method. |
VB Syntax |
measData.putNAComplex location, numPts, data, [format] |
Variable |
(Type) - Description |
|
measData |
An IArrayTransfer interface which supports the Measurement object |
|
location |
(enum NADataStore) Where the Data will be put. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult 3 - naRawMemory 4 - naMemoryResult 5 - naDivisor - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. |
|
numPts |
(long integer) - Number of data points in the channel |
|
data |
(NAComplex) - A one-dimensional array of Complex data matching the number of points in the current measurement. |
|
format |
(enum NADataFormat) - Optional argument. Format of the data. If unspecified, naDataFormat_Polar is assumed. Only used when the destination store is naMeasResult or naMemoryResult. 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Dim measData As IArrayTransfer |
C++ Syntax |
HRESULT putNAComplex(tagNADataStore DataStore, long lNumValues, TsComplex* pArrayOfComplex, tagDataFormat displayFormat) |
Interface |
IArrayTransfer |