Write-only |
About Cal Sets |
Description |
Puts standard acquisition data into the Cal Set. Learn more about Reading and Writing Cal Data |
VB Syntax |
ICalData3.PutStandardComplexByString(stdName, lnumPoints , real(o) , imag(0)) |
Variable |
(Type) - Description |
|
ICalData3 |
An ICalData3 pointer to a Cal Set object. |
|
stdName |
(String) The string used to identify a particular standard in the Cal Set. An example string requesting the data for the Load standard in a full 2 port cal might be "S11C(3,3)". |
|
lnumpoints |
(long) - The number of data points in the real and imaginary arrays. |
|
real |
(Single) The real component of the complex data. |
|
imag |
(Single) The imaginary component of the complex data. |
Return Value |
Single |
Default |
Not Applicable |
Examples |
|
C++ Syntax |
HRESULT PutStandardComplexByString( BSTR bufferName, long lnumPoints, float* real, float* imag); |
Interface |
ICalData3 |