Write-only |
About Cal Sets |
Description |
Note: This command is replaced by PutStandardByString Writes variant data to the error correction buffer holding measurement data acquired for a specific standard. |
|||||||||||||||||||
VB Syntax |
cal.putStandard class,rcv,src,data |
|||||||||||||||||||
Variable |
(Type) - Description |
|||||||||||||||||||
|
cal |
A Calibrator (object) |
|||||||||||||||||||
|
class |
(enum NACalClass) Standard. Choose from:
|
|||||||||||||||||||
|
rcv |
(long) - Receiver Port |
|||||||||||||||||||
|
src |
(long) - Source Port |
|||||||||||||||||||
|
data |
(variant) Two dimensional array (0:1, 0:points-1) |
|||||||||||||||||||
Return Type |
Not Applicable |
|||||||||||||||||||
Default |
Not Applicable |
|||||||||||||||||||
Examples |
Dim varStd (1,200) As Variant |
|||||||||||||||||||
C++ Syntax |
HRESULT raw_putStandard(tagNACalClass stdclass, long ReceivePort, long SourcePort, VARIANT varData) |
|||||||||||||||||||
Interface |
ICalibrator |