Read-only |
About VISAPassthrough |
Description |
Returns data from the VISA pass-through device as a Safe Array of variants. Note that binary data transfers over sockets are not supported. |
VB Syntax |
value = Vpassthru.ReadBinary (visaID) |
Variable |
(Type) - Description |
|
value |
(variant) - Variable to store the returned data. |
|
Vpassthru |
(object) - A VISAPassthrough object |
visaID |
(long) VISA session number (see Open method). |
Return Type |
Safe Array of variants |
Default |
Not Applicable |
Examples |
value=Vpassthru.ReadBinary(1) |
C++ Syntax |
HRESULT ReadBinary(long session_num) |
Interface |
IVISAPassthrough |