Read-only |
About the ExtTestSetIO connector |
Description |
Reads a 13-bit data word from the specified address. Data is read using the AD0 through AD12 lines of the external test set connector. The instrument generates the appropriate timing signals. It automatically controls timing signals LDS, LAS and RLW to strobe the address, and then read the data, from the external test set. See the timing diagram for Address and Data I/O read. |
VB Syntax |
value = ExtIO.ReadData (address) |
Variable |
(Type) - Description |
|
value |
(variant) - Variable to store the returned data |
|
ExtIO |
(object) - An ExternalTestSetIO object |
|
address |
(variant) - address to read data from. |
Return Type |
Variant |
Default |
Not Applicable |
Examples |
value = ExtIO.ReadData (15) |
C++ Syntax |
HRESULT ReadData (VARIANT Address, VARIANT* Data); |
Interface |
IHWExternaTestSetIO |