Read-only |
About the ExtTestSetIO connector |
Description |
Reads a 16-bit value from the external test set. The 16-bit value is comprised of lines AD0 - AD12, Sweep Holdoff In and Interrupt In (inverted). When this command is used the analyzer does NOT generate the appropriate timing signals; it simply reads the lines. The user needs to first use the WriteRaw method to do the initial setup. The RLW line (pin25) must be set to the appropriate level in order to read the test set connected. Below is the format of data that is read with ReadRaw:
|
|
|
Pin |
Bit |
Signal name |
|
|
22 |
0 |
AD0* |
|
|
23 |
1 |
AD1* |
|
|
11 |
2 |
AD2* |
|
|
10 |
3 |
AD3* |
|
|
9 |
4 |
AD4* |
|
|
21 |
5 |
AD5* |
|
|
20 |
6 |
AD6* |
|
|
19 |
7 |
AD7* |
|
|
6 |
8 |
AD8* |
|
|
5 |
9 |
AD9* |
|
|
4 |
10 |
AD10* |
|
|
17 |
11 |
AD11* |
|
|
3 |
12 |
AD12* |
|
|
2 |
13 |
Sweep Holdoff In |
|
|
13 |
14 |
Interrupt In (inverted internally) |
|
|
na |
15 |
Always Zero, grounded internally |
|
|
*These lines are dependent on the state of RLW (pin25). |
VB Syntax |
value = ExtIO.ReadRaw (address) |
Variable |
(Type) - Description |
|
value |
(variant) - Variable to store the returned data |
|
ExtIO |
(object) - An External IO object |
|
address |
(variant) - Address to read data from |
Return Type |
Real |
Default |
Not Applicable |
Examples |
value = ExtIO.ReadRaw (address) |
C++ Syntax |
HRESULT ReadRaw( VARIANT* Input ); |
Interface |
IHWExternalTestSetIO |