Write-only |
About Dynamic Uncertainty |
Description |
Loads an uncertainty ‘workspace’ (*.ml4) file into the Uncertainty Manager. |
VB Syntax |
uncertMan.Recall (fileName) |
Variable |
(Type) - Description |
|
uncertMan |
An UncertaintyManager Object |
|
fileName |
(String). Filename and *.ml4 extension of the Uncertainty Manager workspace file to load. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
uncertMan.Recall"MyWorkspace.ml4" |
C++ Syntax |
HRESULT Recall([in] BSTR fileName); |
Interface |
IUncertaintyManager |