Write only |
About ECal User Characterization |
Description |
Saves the User Characterization to the ECal module. This can take several minutes to complete. To save to VNA disk memory, use SaveToDiskMemory Method. User Characterization can be saved to both VNA disk memory and ECal module memory. |
VB Syntax |
userChar.SaveToECal |
Variable |
(Type) - Description |
|
userChar |
An ECalUserCharacterizer (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
userChar.SaveToECal |
C++ Syntax |
HRESULT SaveToECal(); |
Interface |
IECalUserCharacterizer |