Write-only |
About Dynamic Uncertainty |
Description |
Saves an uncertainty ‘workspace’ (*.ml4) file from the Uncertainty Manager. |
VB Syntax |
uncertMan.Save (fileName) |
Variable |
(Type) - Description |
|
uncertMan |
An UncertaintyManager Object |
|
fileName |
(String). Filename and *.ml4 extension of the Uncertainty Manager workspace file to save. If filename is omitted or NULL (0) is passed for this argument, then Uncertainty Manager’s current workspace is saved to whichever filename that current workspace had been recalled from, even if changes had been made to the workspace since that last Recall. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
uncertMan.Save "MyWorkspace.ml4" 'saves to the specified workspace filename. uncertMan.Save 'saves to the current workspace filename. |
C++ Syntax |
HRESULT Save([in, defaultvalue(0)] BSTR fileName); |
Interface |
IUncertaintyManager |