Write-only |
About Balanced Measurements |
Description |
For a single port balanced device type, maps the VNA ports to the DUT ports. Set the Balanced device type using the DUTTopology Property |
VB Syntax |
balTopology.SetBPort balanced_pos, balanced_neg |
Variable |
(Type) - Description |
|
balTopology |
A BalancedTopology (object) |
|
balanced_pos, balanced_neg |
(Long Integer) VNA port number that connects to each of the following DUT ports: |
Return Type |
Not applicable - To read port mappings, use the BalancedTopology properties. |
Default |
Not Applicable |
Examples |
balTopology.SetBPort 1,2 |
C++ Syntax |
HRESULT SetBPort(long Pos, long Neg) |
Interface |
IBalancedTopology3 |