Write-only |
About Marker Functions |
Description |
Sets the CW frequency to the frequency of the active marker. Does NOT change sweep type. Use ONLY when the current sweep type is sweeping frequency - NOT available in CW or Power Sweep. Use this command to first set the CW Frequency to a value that is known to be within the current calibrated range, THEN set Sweep Type to naPowerSweep or naCWTimeSweep. |
VB Syntax |
mark.SetCWFreq |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
mark.SetCWFreq |
C++ Syntax |
HRESULT SetCWFreq() |
Interface |
IMarker3 |