Write/Read |
About Analyzer Events |
Description |
When set TRUE, configures the analyzer to report outOfRange conditions with an error code. Any overrange error will return E_NA_LIMIT_OUTOFRANGE_ERROR. Note: This method is for the benefit of VB clients. The analyzer automatically adjusts overrange conditions to the closest acceptable setting. The VB user will not See that an overrange occurred because the HRESULT is not returned if it has a success code. For more information, See Events/OverRange. |
VB Syntax |
app.SetFailOnOverRange state |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
state |
(boolean) - |
Return Type |
Not Applicable |
Default |
False (0) |
VB Example |
app.SetFailOnOverRange TRUE ERRHANDLER: |
C++ Syntax |
HRESULT put_SetFailOnOverRange(VARIANT_BOOL mode) |
Interface |
IApplication |