Write-only |
About LXI |
Description |
Modifies settings of the VNA computer networking configuration. |
VB Syntax |
app.SetIPConfiguration AutoIPAddress, DNSServer1, DNSServer2, HostName, DomainName, IPAddress, SubNet, Gateway, DNSSuffix1, DNSSuffix2 or retStr = app.SetIPConfiguration (AutoIPAddress, DNSServer1, DNSServer2, HostName, DomainName, IPAddress, SubNet, Gateway, DNSSuffix1, DNSSuffix2) |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
AutoIPAddress |
(boolean) -Choose either: True - VNA is assigned an IP address by a DHCP server, or will use AutoIP (Dynamic Link-Local Addressing) if DHCP server not found. False – VNA will use the static IP address value specified by IPAddress. |
|
DNSServer1 |
(string) IP address of primary DNS server. When AutoIPAddress = True and an empty string is specified for DNSServer1, the VNA will attempt to obtain the addresses of primary and secondary DNS servers automatically. When AutoIPAddress = False, an IP address must be specified for DNSServer1 and/or DNSServer2 or else the VNA’s host name will not be resolvable on the computer network. |
|
DNSServer2 |
(string) IP address of secondary DNS server. When specifying an empty string for DNSServer1, then specify an empty string here also. |
|
HostName |
(string) DNS host name (computer name) to be assigned to this VNA. Note: If specifying a name different than the VNA’s current host name, the change will not take effect until after you reboot the VNA. |
|
DomainName |
(string) DNS domain name associated with this VNA. |
|
IPAddress |
(string) Static IP address to assign to this VNA when AutoIPAddress = False. When AutoIPAddress = True, the value of IPAddress is ignored. |
|
SubNet |
(string) Subnet mask value to assign to the VNA network configuration. |
|
Gateway |
(string) Gateway address to assign to the VNA network configuration. |
|
DNSSuffix1 |
(string) Primary suffix to set in the VNA DNS suffix search order. An empty string is allowed. |
|
DNSSuffix2 |
(string) Secondary suffix to set in the VNA DNS suffix search order. An empty string is allowed. |
|
retStr |
(string) String returned by this method should be ignored. It is intended for Keysight diagnostic use. |
Return Type |
String |
Default |
Not Applicable |
Examples |
app.SetIPConfiguration True, “”, “”, “MyHostName”, “MyRegion.MyCompany.com”, “”, “255.255.255.0”, “123.45.67.890”, “”, “” app.SetIPConfiguration False, “123.456.78.90”, “234.56.78.901”, “MyHostName”, “MyRegion.MyCompany.com”, “123.456.789.0”, “255.255.255.0”, “123.45.67.890”, “MyCompany.com”, “” |
C++ Syntax |
HRESULT SetIPConfiguration(VARIANT_BOOL AutoIPAddress, BSTR DNSServer1, BSTR DNSServer2, BSTR HostName, BSTR DomainName, BSTR IPAddress, BSTR SubNet, BSTR Gateway, BSTR DNSSuffix1, BSTR DNSSuffix2, BSTR *pRetStr); |
Interface |
IApplication14 |