Write-only |
About VISAPassthrough |
Description |
Sets the timeout value (in milliseconds) for subsequent pass-through commands for the specified VISA session. |
VB Syntax |
Vpassthru.SetVISATimeout visaID, timeoutVal |
Variable |
(Type) - Description |
|
Vpassthru |
(object) - A VISAPassthrough object |
visaID |
(long) VISA session number (see Open method). |
timeoutVal |
(long) Timeout value for the specified session identification number that is used when communicating with this device. |
Default |
2000 |
|
Examples |
Vpassthru.SetVISATimeout 2,6000 |
C++ Syntax |
HRESULT SetVISATimeout(long session_num, long timeout) |
Interface |
IVISAPassthrough |