Write-only |
About Path Configurator |
Description |
Saves the path configuration currently associated with channel (ch) to the specified configuration name. This command is identical to PathConfigurationManager.StoreConfiguration Method |
VB Syntax |
pathMgr.StoreConfiguration ch, name |
Variable |
(Type) - Description |
|
pathMgr |
PathConfigurationManager (object) |
|
ch |
(Long) Channel number of the configuration to be saved. |
|
name |
(String) Configuration name. Factory configurations can NOT be overwritten. Specifying the name of a pre-defined factory configuration will result in an error. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
path.StoreConfiguration(2) "myMixer" |
C++ Syntax |
HRESULT StoreConfiguration( long channelNum, BSTR configName ); |
Interface |
IPathConfigurationManager |