Write-only |
About VISAPassthrough |
Description |
Sends binary data to the VISA pass-through device. Note that binary data transfers over sockets are not supported. |
VB Syntax |
Vpassthru.WriteBinary visaID, bin_data |
Variable |
(Type) - Description |
|
Vpassthru |
(object) - A VISAPassthrough object |
visaID |
(long) VISA session number (see Open method). |
bin_data |
(variant) Data to be sent to the VISA pass-through device. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Vpassthru.WriteBinary 2,"*IDN?" |
C++ Syntax |
HRESULT WriteBinary(long session_num, variant bin_data) |
Interface |
IVISAPassthrough |