Write-only |
About the ExtTestSetIO connector |
Description |
Writes a 13-bit value to the specified address using the AD0 through AD12 lines of the external test set connector. The VNA generates the appropriate timing signals. It automatically controls timing signals LDS, LAS and RLW to strobe the address, then the data, to the external test set. See the timing diagram for Address and Data I/O read. |
VB Syntax |
ExtIO.WriteData address, value |
Variable |
(Type) - Description |
|
ExtIO |
(object) - An External IO object |
|
address |
(variant) - Address to be written to. |
|
value |
(variant) - 13-bit word to write |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
ExtIO.WriteData 15,12 |
C++ Syntax |
HRESULT WriteData(VARIANT Address, VARIANT Data); |
Interface |
IHWExternaTestSetIO |