Write-only |
About VISAPassthrough |
Description |
Sends ASCII string data to the VISA pass-through device. |
VB Syntax |
Vpassthru.WriteString visaID, text |
Variable |
(Type) - Description |
|
Vpassthru |
(object) - A VISAPassthrough object |
visaID |
(long) VISA session number (see Open method). |
text |
(string) Text to be sent to the VISA pass-through device (usually a command). |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Vpassthru.WriteString 2,"*IDN?" |
C++ Syntax |
HRESULT WriteString(long session_num, string text) |
Interface |
IVISAPassthrough |