Read-only |
About the Handler IO Connector |
Description |
Returns the value from the specified "readable" port. |
VB Syntax |
data = handlerIo.get_Port (port) |
Variable |
(Type) - Description |
|
data |
(variant) - A variable to store the return value. The following table shows what the returned data represents: |
|
|
Port |
MSB...........................................LSB |
|
|
C |
C3...C0 |
|
|
D |
D3...D0 |
|
|
E |
D3...D0 + C3...C0 |
|
handlerIo |
(object) - A HandlerIO object |
|
port |
(enum as NAMatHandlerPort) - port to get data from. Choose from: naPortC - (2) naPortD - (3) naPortE - (4) Note: Reading data from the Write-only ports (A,B,F,G,H) will return an error. |
Return Type |
Variant |
Default |
0 |
Examples |
data = handlerIo.get_Port(naPortC) |
C++ Syntax |
HRESULT get_Port ( tagNAMatHandlerPort Port, VARIANT* Data ); |
Interface |
IHWMaterialHandlerIO |