Description
A collection object that provides a mechanism for iterating through the PowerSensor objects which are connected to the power meter. Each time this collection object is accessed, the power meter is queried to determine how many sensors are connected to it. The collection size and order of objects is then adjusted accordingly before the requested method or property operation is performed. The power meter is specified by using the PowerMeterGPIBAddress property of the SourcePowerCalibrator object.
Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim PwrSensors As PowerSensors
Set PwrSensors = app.SourcePowerCalibrator.PowerSensors
Methods |
Description |
|---|---|
|
Use to get a handle to a PowerSensor object in the collection. |
|
Properties |
Description |
|
Returns the number of objects in the collection. |
|
|
Returns a handle to the Parent object (SourcePowerCalibrator) of this collection. |