Write/Read |
About Trigger |
Description |
Determines what happens to an EDGE trigger signal if it occurs before the VNA is ready to be triggered. (LEVEL trigger signals are always ignored.) For more information, see External triggering. |
VB Syntax |
trigsetup.AcceptTriggerBeforeArmed = boolean |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup2 (object) |
|
boolean |
Choose from: False - A trigger signal is ignored if it occurs before the VNA is ready to be triggered. True - A trigger signal is remembered and then used when the VNA becomes armed (ready to be triggered). The VNA remembers only one trigger signal. |
Return Type |
Boolean |
Default |
False |
Examples |
trigsetup.AcceptTriggerBeforeArmed = True 'Write |
C++ Syntax |
HRESULT get_AcceptTriggerBeforeArmed( BOOL *pVal); HRESULT put_AcceptTriggerBeforeArmed( BOOL newVal); |
Interface |
ITriggerSetup2 |