Read-Only |
About Acquisition Time |
Description |
Returns the LO acquisition time which is the ADC Record Size x ADC Sampling Frequency (10 nsec or 40 nsec) x (1 + Stacking) x (Video Average.Coefficient). |
VB Syntax |
value = sa.AcquisitionTime |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Double) Variable to store the returned number of LOs. |
Return Type |
Double |
Default |
N/A |
Examples |
value = sa.AcquisitionTime 'Read |
C++ Syntax |
HRESULT get_AcquisitionTime(double* val); |
Interface |
ISpectrumAnalyzer |