Read-only |
About Markers |
Description |
Returns a handle to the Active Marker object. You can either (1) use the handle directly to access Marker properties and methods, or (2) set a variable to the Marker object. The variable retains a handle to the original object if another Marker becomes active. |
VB Syntax |
1) meas.ActiveMarker.<setting> |
Variable |
(Type) - Description |
|
meas |
(object) - An Measurement object |
|
<setting> |
A marker property (or method) and arguments |
|
mark |
(object) - A marker object |
Return Type |
marker object |
Default |
None |
Examples |
Public mark as marker |
C++ Syntax |
HRESULT get_ActiveMarker(IMarker** marker) |
Interface |
IMeasurement |