Write/Read |
About X-axis display |
Description |
For FCA and GCX measurements, sets the swept parameter to display on the X-axis This command does not change the default setting for new traces. Use Converter.ActiveXAxisRange to change all existing traces and make the setting the default setting for new traces. This command is NOT used for NFX, IMDX, and IMSX measurements. Use Converter.ActiveXAxisRange. |
VB Syntax |
mixer.ActiveXAxisRange = value |
Variable |
(Type) - Description |
|
mixer |
A Mixer (object) |
|
value |
(Enum as MixerStimulusRange) - Parameter to display on the X-axis. Choose from: 0 - mixINPUT - Input frequency span 1 - mixLO_1 - First LO frequency span 2 - mixLO_2 - Second LO frequency span 3 - mixOUTPUT - Output frequency span |
Return Type |
Enum |
Default |
OUTPUT |
Examples |
mixer.ActiveXAxisRange = 1 'Write variable = mixer.ActiveXAxisRange 'Read |
C++ Syntax |
HRESULT get_ActiveXAxisRange(tagMixerStimulusRange *Val) HRESULT put_ActiveXAxisRange(tagMixerStimulusRange newVal) |
Interface |
IMixer3 |