Write-only |
About DIQ |
Description |
Sets the information to display on the X-axis of the selected DIQ measurement. This command does not change the default setting for new traces. See Also: |
VB Syntax |
diqMeas.ActiveXAxis (domain) = source |
Variable |
(Type) - Description |
|
diqMeas |
A DIQMeas (object) |
|
domain |
(Enum as NAAxisDomainType) - Domain to display on the X-axis. Choose from: 0 – naFrequency - display the primary frequency range. 1 – naPower - display the power sweep range 2 – naPhase - display the phase sweep range 3 – naDCValue - display the DC sweep range 4 – naPoints - display the data points in the range |
|
source |
(String) Specific source for the selected domain. |
Return Type |
Enum |
Default |
0 – naFrequency |
Examples |
diqMeas.ActiveXAxis(1) = "Port 2" 'Write variable = diqMeas.ActiveXAxis(1) 'Read |
C++ Syntax |
HRESULT put_ActiveXAxis(tagNAAxisDomainType domainType, BSTR source); |
Interface |
IDifferentialIQMeas |