Read-only |
About Channels |
Description |
Returns a handle to the Active Channel object. You can either (1) use the handle directly to access channel properties and methods, or (2) set a variable to the channel object. The variable retains a handle to the original channel if another channel becomes active. |
VB Syntax |
(1) app.ActiveChannel.<setting> |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
app |
An Application (object) |
|
<setting> |
A channel property (or method) and arguments |
Return Type |
Channel object |
Default |
Not applicable |
Examples |
1) app.ActiveChannel.Averaging = 1 |
C++ Syntax |
HRESULT get_ActiveChannel( IChannel* *pVal) |
Interface |
IApplication |