Write/Read |
About External DC Devices |
Description |
Sets and returns the After Sweep command for an external DC Source and an external DC Meter. |
VB Syntax |
extDC.AfterSweepCmd = value |
Variable |
(Type) - Description |
|
extDC |
A ExternalDCDevice (object) |
|
value |
(String) The SCPI command to be sent at the end of a sweep. |
Return Type |
String |
Default |
" " Empty String |
Examples |
extDC.AfterSweepCmd = "OUTP OFF" 'Write value = extDC.AfterSweepCmd 'Read |
C++ Syntax |
HRESULT get_AfterSweepCmd( BSTR* cmd); HRESULT put_AfterSweepCmd( BSTR cmd); |
Interface |
IExternalDCDevice3 |