Write/Read |
About Segment Sweep |
Description |
Enables you to setup a segment sweep with arbitrary frequencies. The start and stop frequencies of each segment can overlap other segments. Also, each segment can have a start frequency that is greater than its stop frequency which causes a reverse sweep over that segment. Learn more about Arbitrary Segment Sweep. |
VB Syntax |
segs.AllowArbitrarySegments = value |
Variable |
(Type) - Description |
|
segs |
A Segments collection (object) |
|
value |
(boolean) False - Prevents the setup of arbitrary segment sweep. |
Return Type |
Boolean |
Default |
False |
Examples |
segs.AllowArbitrarySegments = True 'Write |
|
AllowArbSegs = AllowArbitrarySegments 'Read |
|
C++ Syntax |
HRESULT get_AllowArbitrarySegments(VARIANT_BOOL *pVal) HRESULT put_AllowArbitrarySegments(VARIANT_BOOL newVal) |
Interface |
ISegments3 |