Write/Read |
About Sweeping |
Description |
Sets sweeps to either alternate or chopped. |
VB Syntax |
object.AlternateSweep = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or CalSet (object) - Read-only property |
|
value |
(boolean) - Choose either: False - Sweep mode set to Chopped - reflection and transmission are measured on the same sweep. True - Sweep mode set to Alternate - reflection and transmission measured on separate sweeps. Improves Mixer bounce and Isolation measurements. Increases cycle time. |
Return Type |
boolean |
Default |
False (0) |
Examples |
chan.AlternateSweep = True 'Write |
|
altSwp = chan.AlternateSweep 'Read |
|
C++ Syntax |
HRESULT AlternateSweep(VARIANT_BOOL *pVal) |
Interface |
IChannel ICalSet3 |