Write/Read |
About Noise Figure |
Description |
Sets and returns the temperature at which the current noise measurement is occurring. Learn more. |
VB Syntax |
noiseCal.AmbientTemperature = value |
Variable |
(Type) - Description |
|
noiseCal |
A NoiseCal (object) |
|
value |
(double) Ambient temperature in Kelvin. |
Return Type |
Double |
Default |
295 |
Examples |
noise.AmbientTemperature = 289'Write |
|
temp = noise.AmbientTemperature 'Read |
|
C++ Syntax |
HRESULT get_AmbientTemperature(Double* pValue) HRESULT put_AmbientTemperature(Double pNewValue) |
Interface |
INoiseCal |